undefined [object Object]
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How do I communicate with multiple ION 7600 over ethernet with DNP3.0?

Issue
DNP3.0 requires a unit ID even if it is over ethernet.

Product Line
ION 7500, ION7600

Environment
IONSetup

Cause
The framework in an ION7600 does not allow you to set the DLAddress for ethernet (which is essentially the unit ID).

Resolution

  1. Set COM2 to Ethergate
    Setup assistant
  2. Connect the twisted shielded pair (RS485) between COM1 and COM2
  3. Set the protocol on COM1 to DNP3.0 then set the unit ID to the desired number.
    Setup com protocol
NOTE: all devices and COM ports must have unique device IDs, and all operate at the same baud rate.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: