Search FAQs
Is the ION 7550/7650 battery field replaceable?
Issue
Is it possible to field retrofit the battery within the ION7550/7650 meters
Product Line
ION7550
ION7650
Environment
Hardware Replacement
Resolution
Yes the battery is field replaceable. Schneider no longer sells this battery, however it can be purchased from Tadiran and the part number is TL-5276/W or equivalent.
The instructions for replacing the battery are attached below.
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: