{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I retro-fit my 73xx series from a normal display to a RMD?

The meter would require full retro-fit (RMA) of all boards to change over to an RMD, this would require the meter to come back to the factory. Contact RMA for details & cost. It is likely more effective for the customer to exchange the meter if it is still un-opened or to keep this meter and buy a Tran/RMD model as well if the display model was previously installed.

Last Revised: November 19, 2007
Applies To: ION 7300/7330/7350
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189305 V1.0, Originally authored by KBAdPM on 11/20/2007, Last Edited by KBAdPM on 11/20/2007
Related ranges: ION7300

Schneider Electric Egypt and North East Africa