This is done through Windows Device Manager.
- Click on the Start Menu > Control Panel > System
- Select the Hardware tab then click Device Manager
- Scroll to the Ports section and expand it
- Right click on the appropriate COM port and select Properties
- Select the Port Settings tab to check the settings (baud, etc). This should match the baud rate on the meter.
Last Revised: November 22, 2007
Public
All content © 1992-2007 Schneider Electric
Legacy KB System (APS) Data: RESL189432 V1.0, Originally authored by KBAdPM on 11/22/2007, Last Edited by KBAdPM on 11/22/2007
Related ranges: third party devices (modems, converters...)
Released for:Schneider Electric Egypt and North East Africa