{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Will ION Enterprise retain Historical data if a Meter node is deleted, then added again later with the same name?

As long as the node names remain the same, the historical data will remain intact since ION_Network and ION_Data reference logged data to the node names. If a device/node is deleted from Management Console, and a new device with the same name is created, that new device will map to the existing data in ION_Data.

Last Revised: November 22, 2007
Applies To: ION Enterprise
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189570 V1.0, Originally authored by KBAdPM on 11/23/2007, Last Edited by KBAdPM on 11/23/2007
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5, ION Enterprise V5.0, ION Enterprise V4.5

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.