{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How To Force a Particular ION Enterprise VISTA Diagram to Open for a Given User on Startup


Summary

In some circumstances, it is desirable to maintain a specific Vista workspace for a particular user, so every time the user logs into Vista, the same set of diagrams are opened.

1) Log on to VISTA using the user account that is to be set up.
2) Organize VISTA to appear as you want it to appear on startup.
3) Save, and close VISTA.
4) Using Windows Explorer, navigate to the ION Enterprise(or PEGASYS)/config/cfg/ud directory. Notice there is a .wsu file named for each user account.
5) Locate the .wsu file for the user account you want to lock down and right click to bring up the Properties dialog box.
6) Mark the file as Read-Only

Now, every time that this user logs into VISTA, the same set of diagrams will be displayed.



Original article#9605 (SWKB-0312)
Date Created: Unknown
Last Revised: May 8, 2009 by MN
Public
Original Author: Unknown
All content © 1992-2009 Schneider Electric

Legacy KB System (APS) Data: RESL189927 V2.0, Originally authored by KBAdPM on 12/03/2007, Last Edited by MiNe on 05/09/2009
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5, ION Enterprise V5.0, ION Enterprise V4.5

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.