Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Which maximum current can the tap off units withstand?

For tap off unit reference n°04151 => In: 35A (6²) et 45A (10²) at 40°C
For tap off unit reference N°04152 => In: 55A (16²) at 40°C

 The current is limited by the cage terminal not by the cable cross section.


Legacy KB System (APS) Data: RESL196279 V2.0, Originally authored by SeOs on 12/31/2008, Last Edited by GwPo on 06/25/2010
Related ranges: Prisma Plus

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.