{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
The E5600 meter will not communicate via RS-485.

If the E5600 meter is installed in switchgear, it is possible to install the communication cable wire harness upside down. The E5600 meter can only communicate if the wire harness is installed the correct direction even though it is possible to install the wire harness upside down if you push hard enough.
The symptoms of this issue include the fact that all the settings in the software are correct. The Tx and Rx lights will not blink at all. The meter will communicate through the optical cable but not RS-485. When the switchgear is opened the communication cable can be very difficult to remove from the meter.

To resolve the issue flip the communications cable 180 degrees such that the cable is then right side up. This will resolve the communications issue and the Tx and Rx lights will begin flashing.


Date Created: July 22, 2009
Last Revised: July 22, 2009
Public
Original Author: MN
All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL199429 V1.0, Originally authored by MiNe on 07/23/2009, Last Edited by MiNe on 07/23/2009
Related ranges: E5600

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.