{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What device types does the EGX300 support?

EGX300 Supported Device Types
ATS48
CM100/200
CM2000
CM3000
CM4000
Compact NSX A
Compact NSX E
Enercept Meter
Energy Meter
ION6200
ION7300
ION7500
ION7550
ION7600
ION7650
Micrologic Type A
Micrologic Type H
Micrologic Type P
Model 98
MotorLogic Plus
MotorLogic Plus II
MVSS/RVSS
PM200
PM300
PM500
PM600
PM700
PM800
Sepam 2000
Sepam Series 20
Sepam Series 40
Sepam Series 80
TeSys T

As of firmware 3.8, the following device types are now additionally supported:
ATV61
ATV71
Accusine
BCM
BCPM - A, B, and C
DM6000
E5600
EM26-96
ION6200 (mega)
ION8600
MCM
PM1000
PM5000
PM9c
Sepam Series 10
Twido BK
Twido-wages
Var Logic

As of firmware 3.81, the following device types are now additionally supported:
SIM10M
SIM10Z
SIM6BZ

As of firmware 3.9, the following device types are now additionally supported:
Micrologic E

As of firmware 3.91, the following device types are now additionally supported:
VigilOhm IM20, IM20-H
Twido-WAGES D12, D28, D44

As of firmware 4.0, the following device types are now additionally supported:
EM1200
DM6300
EM6400
EM6433
EM6436
EM6438
PowerPact A
PowerPact E
4-noks ZED-THL-M

As of firmware 4.2and disk update version 4.210, the following device types are now additionally supported:

iEM3150
iEM3155
iEM3250
iEM3255
EM3550
EM3555
Acti9 SmartLink
EM1200
EM1250
EM1251
PM3250
PM3255

As of firmware 4.3, the following device types are now additionally supported:

EM7320
EM7380
PM5350BW

As of firmware 4.35 and disk update 4.360, the following device types are now additionally supported:

PM5100/PM5300 series meters
EM4800
PM5560
Conext TL

As of firmware 4.37 and disk update 4.37, the following device types are now additionally supported:
IM400
iEM3350
iEM3355

As of firmware 4.38 and disk update 4.38, the following device types are now additionally supported:
EM1350

As of firmware 4.40 and disk update 4.40, the following device types are now additionally supported:
Micrologic A IFE/IFM
Micrologic P IFE/IFM
Micrologic H IFE/IFM
Micrologic E IFE/IFM
Micrologic A IFE IO1
Micrologic P IFE IO1
Micrologic H IFE IO1
Micrologic E IFE IO1
Micrologic A IFE IO2
Micrologic P IFE IO2
Micrologic H IFE IO2
Micrologic E IFE IO2
IFE IO1
IFE IO2
Compact NSX-A IO1,
Compact NSX-E IO1
Compact NSX-A IO2
Compact NSX-E IO2
PowerPact A IO1
PowerPact E IO1
PowerPact A IO2
PowerPact E IO2
BCPM-Model A/E
Acti 9 Smartlink Ethernet
EM6400NG/PM2xxx


Article Updates
MT 8/23/2012 - Added additional device support with disk update 4.210
MT 3/12/2013 - Added 4.3 device support
MT 1/13/2014 - Added 4.35 device support
4/17/2015 - Added 4.36 and 4.37 device support
8/5/2015 - Added 4.40 device support

Schneider Electric Egypt and North East Africa