{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the username and password for the E4800 and EM4800 Config Tool?

Issue
What is username and password for the EM4800 configuration tool

Product Line
EM4800
E4800

Environment
Software Passwords

Resolution
The username and password for the E4800 and EM4800 Config Tool are:

Username: PowerLogic
Password: E4800

Username/password are case sensitive.

For more information about these meters see FA212909

To download the EM4800 configuration tool, please see the following FAQ FA369955

Schneider Electric Egypt and North East Africa