{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the control power burden rating of a PowerLogic meter, ION meter or Sepam Relay?

Issue
Control power specifications of the various meters

Product Line
Sepam 10, Sepam 20, Sepam 40, Sepam 80, CM2000 (CM2), CM3000 (CM3), CM4000 (CM4), CM4ECC (ECC21), PM1000, PM210 (PM2), PM700 (PM7), PM800 (PM8), PM5000, PM8000, ION6200, ION7300, ION7550, ION7650, ION8600, ION8650, Enercept Meter, Energy Meter, SMD63, EM4805

Environment
Metering application requiring control for the metering devices

Cause
Need to select power supply to power meters

Resolution
The burden ratings for the Powerlogic, ION, and SEPAM devices are outlined in the attached EXCEL spreadsheet.

Schneider Electric Egypt and North East Africa

Attachment(s)
burden_ratings.xls [26 KB]