{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to upgrade firmware on a PowerLogic E4800 and EM4800

Issue
How to upgrade firmware on a PowerLogic E4800 and EM4800

Product Line
E4800, EM4800

Environment
Firmware downloader

Cause
A Schneider firmware downloader was developed as an easy method to upgrade the meters.

Resolution
As of 9/28/2018, the latest firmware  is V2.05 Build 1217. This firmware is relevant for both the EM4800 and E4800.

A Schneider firmware downloader was developed as an easy method to upgrade the meters. Below you can find the firmware file, the Schneider firmware loader. The tool does not require installation. It can run simply by unpacking the ".zip into a folder of your choice. Also attached is a very brief and preliminary version of an instruction document (Schneider_firmware_Loader.pdf).

Warning: The firmware utilities listed here can cause permanent damage to your product if applied incorrectly. Before downloading any firmware updates, verify the firmware you are downloading is appropriate for the specific model number of your product. If you have any doubts, contact Technical Support for guidance.

*Warning: Be sure all other software, is not connected to the meter.*


NOTE: A firmware upgrade will reset the energy readings for all the circuits.

Follow the steps in the .pdf to upgrade the EM4800 firmware using the attached files.

Schneider Electric Egypt and North East Africa

Attachment(s)

Schneider_firmware_Loader.pdfSchneider_firmware_Loader.pdf [475.96 KB]
PH6X12-FW-V2.05-build1217.zipPH6X12-FW-V2.05-build1217.zip [403.04 KB]
SchneiderFwmDownloader_1.0.0.23.zipSchneiderFwmDownloader_1.0.0.23.zip [170.49 KB]
Explore more
Range:
EM4000 series
Explore more
Range:
EM4000 series
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.