{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Understanding the PowerLogic Drivers (PWRMODBUS, PLOGIC, SEPAM, MICROLOGIC) as Backend Drivers Which Use a Cache and Poll All Configured Variable Tags Continuously

It is important to note that PowerLogic SCADA's PowerLogic drivers (PWRMODBUS, MICROLOGIC, PLOGIC, SEPAM) are "backend" drivers, that is to say, they poll I/O devices through a cache. Previously, with most Citect drivers, one could configure the Cache and Cache Time parameters for a given I/O device. With the PowerLogic drivers, caching is the default operation.
When Runtime is started, all I/O devices using the PowerLogic drivers attempt to populate the cache with data for all Variable Tags configured for those devices. This is why a user may see some delay between Runtime is started and when data is available on all graphic pages. Once the cache is fully populated, the drivers attempt to keep that data updated based on the interval specified by the CacheRefreshTime citect.ini parameter. Settings like the scan time and poll time do not affect the device polling as they did for previous drivers. Regardless of the presence of alarm tags, variable tags are polled based on a combination of the CacheRefreshTime and Bandwidth parameters. Values are always taken from the driver's cache. More information about the aforementioned parameters can be found in the PowerLogic SCADA System Integrator's Manual.


Keywords: PLS, PL SCADA, PLSCADA, PowerSCADA, 7.10, 7.20, v7.10, v7.20, 710, 720, back end, poll all tags all the time


Legacy KB System (APS) Data: RESL207051 V1.0, Originally authored by AnVa on 01/05/2012, Last Edited by AnVa on 01/05/2012
Related ranges: PowerLogic SCADA 7.20, PowerLogic SCADA 7.1

AEDL3

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.