{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What device types are supported in ION Enterprise 6.0?

Issue
Which devices and device drivers are supported in ION Enterprise 6.0 SP1?

Product Line
ION Enterprise 6.0 SP1

Environment
Device Driver for ION Enterprise 6.0 SP1

Resolution
ION 6.0 SP1 Natively supported device types:


3300 ACM
3710 ACM
3720 ACM
3800 RTU
Access 9200
Access 9200 (Modbus)
Access 9300
Access 9330
Access 9350
Access 9500
Access 9500 RTU
Access 9510
Access 9510 RTU
Access 9600
Access 9610
Access 9700
BCPM
CM2000 Series
CM3000 Series
CM4000 Series
DM6200
EM5600
ION 6200
ION 6200 (Modbus)
ION 7300
ION 7330
ION 7350
ION 7500
ION 7500 RTU
ION 7550
ION 7550 RTU
ION 7600
ION 7650
ION 7700
ION 8300
ION 8400
ION 8500
ION 8600
ION 8800
Micrologic A Compact NSX
Micrologic E Compact NSX
Micrologic H
Micrologic P
Mircologic A
PM1200
PM200
PM700
PM800
Sepam series 10
Sepam series 20
Sepam series 40
Sepam series 48

LE (Limited Edition) Drivers available for:

BCM42
CM100-200
Enercept Meter
Energy Meter
MCM
Model 98
PM500
PM600
Sepam 2000
Motor Logic Plus
TeSysT

The LE optional device drivers available for installation into ION Enterprise 5.6 SP2 and 6.0 can be downloaded from the link below:
http://www2.schneider-electric.com/sites/corporate/en/products-services/former-brands/powerlogic/powerlogic_optional_device_drivers.page

Note: The optional device drivers listed below will only install on ION Enterprise 5.6 SP2 and 6.0. Earlier versions of ION Enterprise are not supported.

Schneider Electric Egypt and North East Africa