{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Error 'COMDLG32.OCX missing' when trying to install Slinger

The following error appears when you are installing Sling on Win 7, Server 2008 or Win 8:


COMCTL32.OCX is an Active X Control that is used by applications to display dialogs. It is widely used, but considered 'old' as it has been replaced in new applications by MS presentation foundation (WPF) . The solution is to reinstall this component.

The description of the problem, how to solve it, and several documents with background information can be found at

http://answers.microsoft.com/en-us/windows/forum/windows_7-files/comctl32ocx-error-in-windows-7/051b2862-b4a1-45fc-aad8-140ed32dc682


Legacy KB System (APS) Data: RESL210067 V1.0, Originally authored by CoBu on 12/18/2012, Last Edited by CoBu on 12/18/2012
Related ranges: Vizelia, REM, EVO, EPO, Hosted Simple Energy Management Solution (SEMS)

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.