{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the NEMA rating for the PowerLogic Energy Meter enclosure?

Issue
User would like to know the enclosure rating for the Powerlogic Energy Meter and if it is suitable for outdoor use.

Product Line
Energy meter
EMBxxxx
EMExxxx

Environment
NEMA enclosure rating

Resolution
​The enclosure for the Energy Meter is NEMA 1 rated.  The Energy Meter is NOT rated for outdoor use.

Definition: from NEMA 250-2003:
Type 1 (NEMA 1) - Enclosures constructed for indoor use to provide a degree of protection to personnel against access to hazardous parts and to provide a degree of protection of the equipment inside the enclosure against ingress of solid foreign objects (falling dirt).

Schneider Electric Egypt and North East Africa