{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to Connect to a MB+ network with Unity Pro on a remote PC using a MBX Gateway?

Connecting Using the MBX Gateway Driver

Facts and Changes

MBX Driver Suite v6.0

Causes and Fixes

Note: For information on how to setup the MBX Gateway Client and Server see the resolution entitled "How to connect remotely to a MB+ network via TCP/IP using the MBX Gateway driver".
To Connect to a MB+ Network with Unity Pro from a remote PC via the MBX Gateway you must chose the Adapter/Device number of the MBX Gateway Client in the Communication Setup.

Under PLC chose Set Address.



Type in the MB+ address of the PLC and under Media chose the MB+ device number of the MBX Gateway Client.
Note: This Number is offset by 1 in Unity. So if your MBX Gateway Client is set as device 1 in the MBX Gateway configuration you would chose MBPLUS02 as the Media.



Press OK and then chose connect from the PLC menu to connect to the PLC.


Schneider Electric Egypt and North East Africa