{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What TCP ports are used in ION Enterprise and StruxureWare Power Monitoring Expert?
Issue
What TCP ports are used by ION Enterprise or StruxureWare Power Monitoring Expert?


Product Line
ION Enterprise, StruxureWare Power Monitoring Expert (PME)


Environment
All ION or PME power monitoring systems


Cause
ION/PME requires certain ports be opened in order for the Software, SQL and Meter Communications to be successful.


Resolution
The following tables show the ports used by ION Enterprise and StruxureWare Power Monitoring Expert, up to and including PME v8.2:



For graphical representation see the diagram, up to and including PME v8.2:

Note: port 1498 is used for Sybase database

The following table lists all relevant ports and their functions for PME v9.0:



The following image shows the ports and the components they are associated with, for PME v9.0:

Schneider Electric Egypt and North East Africa