This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Please refer the attachment for the connection terminal details.
1. The analog input of 4-20mA from PLC to VFD should be connected between terminals AI2 & COM. The reference channel-1 should be programmed for AI2 and the parameter AI2 configuration should be programmed for 4 to 20mA.
2. The Analog output of 4 to 20mA from VFD to PLC should be connected between terminals AO1 & COM. The analog output assignment and scaling can be done through parameters as shown in the attachment.
Released for: Schneider Electric Egypt and North East Africa