Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What's the meaning of "Maximum prospective short-circuit current of the Soft Starter/Drive according to standard IEC 60947-4-2" ?
The prospective short circuit current is the highest current which can exist in particular electrical system under short circuit conditions.

As per IEC60947-4-2:

路         Type 1 coordination: allows the product to be damaged during short circuit condition, hence the product can be used again.

路         Type 2 coordination: does not allow the product to get damaged, the product can be re-used after clearing the fault.

The maximum prospective short circuit current value is provided for the combination given, supply voltage, type of coordination (1 or 2) available in the catalog of each Soft starter/Drive range.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more