{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Power Monitoring Expert and USB Modems

Issue
User does not have a Physical COMM port on the machine running Power Monitoring Expert (PME) Software

Product Line
Power Monitoring Expert

Environment
Physical Servers

Cause
Not recommended to use a USB to Serial converter dongle.

Resolution
Two main options for connecting modems to a physical server without a COMM port.

1) Add an internal PCI card with serial ports example (http://www.comtrolstore.com/RocketPort_Express_PCIe_4_Port_s/413.htm)

2) USB to Serial converter such as http://www.digi.com/products/usb/edgeport#models

Schneider Electric Egypt and North East Africa