{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
EN50160 Advanced PQ Error ‘ION Object Does Not Exist’

Goals and Symptoms

Summary


  • This KB is only valid for meters that were ordered with the Special Order Option of EN50160 compliance. The 7650, 8600A, 8800A, 8800B are currently the only EN50160 Power Quality meters.

    Advanced Power Quality meters can cause an error in Vista if the PQ framework is not setup correctly. The error is caused by the incorrect framework (non PQ framework) installed on the meter. To recover, the PQ framework must be placed on the meter, then the proper setup procedure must be followed to enable the Advanced PQ functions of the device.

    The problem produces the error ION Object Does not Exist



    Keywords

    Vista, PQ, Power Quality, EN50160, Error, Setup, Framework, 7650, 7550, 8600, ION Object Does not Exist

Causes and Fixes

See attached ION Knowledge Base article.
EN50160 Advanced PQ Error ION Object Does Not Exist.pdf

Schneider Electric Egypt and North East Africa