Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
What type of 10Base-FL Fiber is Required for devices with fiber optic communications?
Issue
What is the best type of 10Base-FL Fiber for 10Base-FL communications

Product Line
ION Devices

Environment
Fiber Optic Communications

Cause
Some devices such as older (pre 2008) models of the ION7650 have a fiber-optic communication hardware ordering option

Resolution
These are the best specifications for the the fiber to be on the 10Base-FL port
* Multi-Mode fiber
* Wavelength: 850 nm
* Connector Type:    ST
* Cladding: 62.5/125 um
* Max Length: 2000m

Note: For 100Base-FX communications see What type of 100Base-FX Fiber is Required for devices with fiber optic communications?

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: