{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How can I share a single CT and PT for two or more Meters?

Issue
The User would like to use a PT (potential transformer) or a CT (current transformer) for two separate meters..

Product Line
PowerLogic and ION Meters

Environment
Current Transformers and Potential Transformers

Cause
Typically each power meter has its own set of CT's and PT's. It may be desirable to share a voltage or current source from one of the PT's or CT's.

Resolution
The ION and PM meters can share CTs and PTs with other meters.


  • Take PM1200 and three phase 4 wire connection for example, the wiring should be like below:
    Wiring Diagram

    Also,this wiring can be used in other PM and ION meters.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: