Search FAQs
171CCC9x0x0 M1E Processor 984LL Exec. Upgrade to v.1.25
Issue
The purpose of this resolution is to inform Momentum M1E users that the 984LL Exec. has been upgraded to version 1.25.
Exec. v.1.25 resolves an issue with pinging an M1E through a router across a WAN. This problem occurred in 984LL Exec. versions 1.21 and 1.23. It did not occur in v.1.20.
Product Line
· 171CCC98030
· 171CCC96030
· 171CCC98020
· 171CCC96020
Resolution
Installing 984LL Exec. v.1.25 resolves the above-mentioned issue.
Note: It is recommended to power cycle the M1E immediately after downloading an Exec.
Legacy KB System (APS) Data: RESL174643 V2.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Momentum
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: