Goals and Symptoms
This resolution contains information which enables users to replace the internal 3AG Fast Acting Glass Body fuses that are in series with AS-B814-108 outputs.
Causes and Fixes
B814 fuses can be accessed by removing a plate which covers the option jumpers. In the illustration the plate has a Caution label on it. Four screws need to be removed to free the plate.
Fuse part numbers: Schneider 57-0083-000
-
-
-
- Littelfuse 312007
Bussman MTH7
- Littelfuse 312007
-
-
Legacy KB System (APS) Data: RESL180177 V1.0, Originally authored by WeDa on 10/23/2006, Last Edited by WeDa on 10/23/2006
Related ranges: Modicon 1/2/3/4/5/8/984s