{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
STBNMP2212 Module Holdup Timeout Register Range

Issue

This resolution documents minimum and maximum values that may be assigned to the STBNMP2212 Module Holdup Timeout Register.
Default value of the timeout register is 100 or 1second. Minimum time that can be set is 300 ms, the maximum time is 60 seconds. Values written beyond the limits will be automatically set back to the limit.

Product Line
Advantys,STB

Resolution

Information regarding the Module Holdup Timeout Register may be found in the Advantys STB Modbus Plus Network Interface Applications Guide, p/n 890USE17800 (33004629) and in Advantys Configuration Software on-line Hardware Help for the MB+ NIM.

Schneider Electric Egypt and North East Africa