{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
171CBB97030 Processor/4 Port Switch IEC Exec. Upgrade to v.1.05

Issue
The purpose of this resolution is to inform 171CBB97030 users that the IEC Exec. has been upgraded (March 2008) to version 1.05, for use with Concept 2.6.


Product Line
Momentum


Resolution
IEC Exec version 1.05 resolves the following issues:

1) Under certain conditions, the M1E would not respond to a second ARP.
2) If two or more MSTR TCP function blocks (i.e. Read_Reg) are programmed in logic, periodically, one of the blocks could freeze operation for 3-5 minutes, then recover on its own.
3) PSH flag is no longer set in the SYN and FIN packets. This caused communication problems between the M1E and a third-party device.
4) Fixes an issue in the M1E web page where the 'TCP Retry' counter would increment every time a TCP MSTR block was activated.


Installing IEC Exec. v.1.05 (filename: mpsv105e.bin) resolves the above-mentioned issues.


Legacy KB System (APS) Data: RESL191608 V2.0, Originally authored by DaDz on 04/04/2008, Last Edited by DaDz on 04/05/2008
Related ranges: Modicon Momentum

Schneider Electric Egypt and North East Africa