{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to restore the RS-485 communications on a 'Tesys U' connected to a Tesysport..

Issue
How to restore the RS-485 communications on a 'Tesys U' connected to a Tesysport.

Product Line
TESYS U

Environment
Windows 7

Resolution
If '140NOE77111 'communications to the Tesysport is recovered after a lockup, the RS-485 connection to
the 'Tesys U' does not get restored. When this happens, the ERR led on the 'Tesys U' will be flashing.

In order to re-establish the RS-485 Modbus communications to the 'Tesys U', the recovery bit (bit 3 of
word 703) must be reset.

The following is from page 58 of the 'TeSys® U LULC032-033 Modbus Communication Module
Users Manual'.

Recovery After Loss of Communication
After acknowledgment by setting bit 703.3 to 1, recovery occurs according to the states of control

bits 704.0 and 704.1.

To resolve the issue the application needs to be modified to

  • Detect a 'Loss of communications with a master warning' using word 109 bit 15 as described on page
58 of the user manual.
  • Set bit 3 of word 703 upon detection of the communications loss.
  • Reset bit 3 of 703 after the 'Loss of communications with a master warning' is cleared.

Legacy KB System (APS) Data: RESL201897 V1.0, Originally authored by AlCh on 12/16/2010, Last Edited by AlCh on 12/16/2010
Related ranges: Modicon Quantum

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: