Issue
The attached document is a CIP Modbus Object Write example for a TSXETC101 using the Send_Req block to write to a Quantum 140NOC77101.
Product Line
This program will read from located registers in Schneider PLC's with the following network modules installed:
- 140NOC77101
- BMXNOC0401
- TSXETC101
- 140NOC78000
Resolution
See attachment: TSXETC101_CIP_Modbus_Object_WRITE_Example.pdf
Legacy KB System (APS) Data: RESL210427 V1.0, Originally authored by DaDz on 01/25/2013, Last Edited by DaDz on 01/25/2013
Related ranges: Modicon Premium
Released for:Schneider Electric Egypt and North East Africa