{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

PowerLogic CM2000 (CM2) Firmware version 17.011 for use with DLF3000 and DLF101 (fix for rapid energy accumulation on previous versions of firmware)

Product Line
CM2000

Environment
Firmware

Resolution
The attached .zip file contains a .fw file for DLF3000 version 3.0, and a .sys and .hex file for DLF101, if needed.

See Video: Firmware upgrade on a PM800, PM5XXX, PM200, PM700, CM4000/T, CM3000 and CM2000 series meters using DLF-3000 for the download for DLF3000 and how to use it.

Note: This is the most up to date version of the firmware for a CM2 series meter.

Schneider Electric Egypt and North East Africa

Attachment(s)

CM2K_Fw_v17_5B1_5D.011.zipCM2K_Fw_v17_5B1_5D.011.zip [300.59 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: