{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ION Enterprise v5.6 Webreach shows blanks (empty boxes) for real time data due to problems with MDAC 2.8 on Windows XP Pro Service Pack 3 (SP3)

Goals and Symptoms

Summary:

Using ION Enterprise 5.6 Service Pack 2 (SP2) on a Windows XP Pro SP3, it is possible that real time data can be updating in Vista, but when Webreach is opened there is no real time data for any meters, just blanks. Repairing MDAC 2.81 has been found to resolve the issue.
Symptoms:

- Real time data in Numeric objects in Webreach show blanks (no N/A or '...')



- All other KB articles for troubleshooting Webreach real time data do not work to resolve this issue.

- No Windows Event log errors

- ION Enterprise Setup log errors can be found to be the cause of real-time data not working.

Facts and Changes

Keywords:

Webreach

Real time Realtime OR Real-time data

Blank OR Blanks

MDAC

Windows XP Pro SP3, SP2

empty boxes

Causes and Fixes

Causes:

Problems with Microsoft's MDAC component in Windows XP.

Fixes:

Follow Method 2 of this Microsoft KB article to repair the MDAC.
http://support.microsoft.com/kb/899861

Excerpt:

  • Method 2: Repair the MDAC 2.81 installation that is included with Windows XP SP2
    • 1. In Windows Explorer, open the c:\Windows\Inf folder.

      Note If you cannot see the c:\Windows\Inf folder, follow these steps:
        • a. Click Start, click My Computer, and then click Folder Options on the Tools menu.
          b. Click the View tab.
          c. Under Advanced settings, click Show hidden files and folders.
          d. Click to clear the Hide extensions for known file types check box.
          e. Click Apply, and then click OK.
      2. In the c:\Windows\Inf folder, right-click the Mdac.inf file, and then click Install.
      3. When you are prompted to insert the Windows XP SP2 CD, use one of the following methods:
            • a. Insert the Windows XP Service Pack 2 CD in the CD or DVD drive.

              Note If a "Welcome to Microsoft Windows XP" message appears, click Exit.
              b. Click Browse.
              c. In the File name box, type CD or DVD drive that contains the Windows XP Service Pack 2 CD drive letter:\i386. For example, type d:\i386 if the Windows XP Service Pack 2 CD is in drive D.
              d. Click Open.
          • In the File name box, type %systemroot%\windows\servicepackfiles\i386, and then click Open.
      4. You may also be prompted for the original Windows XP CD that was used to install the operating system.
        • a. Insert the Windows XP Service Pack 2 CD in the CD or DVD drive.

          Note If a "Welcome to Microsoft Windows XP" message appears, click Exit.
          b. Click Browse.
          c. In the File name box, type CD or DVD drive that contains the Windows XP Service Pack 2 CD drive letter:\i386. For example, type d:\i386 if the Windows XP Service Pack 2 CD is in drive D.
          d. Click Open.

Attachments

(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/c3888b97d39e39a3c125755b00583202/fl_block_5/0.3070?OpenElement&FieldElemFormat=gif)

  • Date Created: December 17, 2008
    Last Revised: February 12, 2009
    Public
    Original Author: EW
    All content © 1992-2009 Schneider Electric

Legacy KB System (APS) Data: RESL197797 V1.0, Originally authored by KBAdPM on 02/12/2009, Last Edited by KBAdPM on 02/12/2009
Related ranges: ION Enterprise V5.6

Schneider Electric Egypt and North East Africa