{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the split rear doors of a NetShelter SX, SV or VX cabinet be installed on the front of the cabinet, and can the front door be installed on the rear?
Issue:
Design of the data center may require a full width door on the rear and/or split doors on the front.

Product Line:
NetShelter SX, NetShelter SV, NetShelter VX

Environment:
All versions and serial ranges.

Cause:
Data center layout requires NetShelter SX, SV or VX cabinet to be flexible and allow the customer to choose what door style is installed in the front and/or rear.

Resolution:
Yes, the rear doors can be installed onto the front of the cabinet and the front doors onto the rear.
When moving the rear doors to the front you must also move one set of hinges from the rear to the front.
Replacement front and rear door kits include all of the hinges necessary to hang the doors.

Schneider Electric Egypt and North East Africa