{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What to do if you cannot SSH into PowerChute Network Shutdown appliance running on VMware?
Issue:
Attempting to SSH to PowerChute Network Shutdown Appliance and receive error message stating that connection has been refused.

Product Line:
PowerChute Network Shutdown Appliance for VMware

Environment:
PowerChute 4.x and 5.x VM running on VMware ESXi host.

Cause:
SSH is not running.

Solution:
Note: All commands are in Bold Italic

Log into the Appliance using VMware vSphere Client.

Check to see if SSH is running. The command is
systemctl status sshd

If the service is not running run this command
systemctl start sshd

If you would like the service to start automatically with the VM enter the command
systemctl enable sshd

Schneider Electric Egypt and North East Africa