Search FAQs
Why the vfd will not ramp to the correct speed of the 0-10V signal on AI1?
Issue:
The analog input signal do not match what is being sent.
Product line:
Altivar 61/71
Environment:
All models, all serial numbers
Cause:
The AI1 input is a bipolar input. If AI1 negative is not referenced to common the drive is looking for a range of 20 V dc ( +10 to - 10).
Resolution:
Verify the factory installed jumper between AI1- and common terminals is installed.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: