{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to choose between EN/ISO 13849 and EN/IEC 62061 ?
Based on the generic definition of the risk, the standards classify necessary safety
levels in different discrete levels corresponding for each one to a probability of
dangerous failure per hour:
>> PL (Performance Level) for standard EN/ISO 13849-1
>> SIL (Safety Integrity Level) for standard EN/IEC 62061

Kindly, Check the attached document.

Schneider Electric Egypt and North East Africa

Attachment(s)
Difference between EN_ISO 13849 and EN_IEC 62061.pdf [371.4 KB]
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to choose between EN/ISO 13849 and EN/IEC 62061 ?
Based on the generic definition of the risk, the standards classify necessary safety
levels in different discrete levels corresponding for each one to a probability of
dangerous failure per hour:
>> PL (Performance Level) for standard EN/ISO 13849-1
>> SIL (Safety Integrity Level) for standard EN/IEC 62061

Kindly, Check the attached document.

Schneider Electric Egypt and North East Africa

Attachment(s)
Difference between EN_ISO 13849 and EN_IEC 62061.pdf [371.4 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
move-arrow-top