This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
The difference between flush and non flush mountable sensor is as below :
Flush-style sensors actually have a shield that restricts the magnetic field so that it only radiates out of the face of the sensor. ... Non-flush, or unshielded sensors, do not have the shield around the end of the sensor so the field can radiate from the face to the sides of the sensor in a larger pattern.
Flush-style sensors actually have a shield that restricts the magnetic field so that it only radiates out of the face of the sensor. ... Non-flush, or unshielded sensors, do not have the shield around the end of the sensor so the field can radiate from the face to the sides of the sensor in a larger pattern.
Released for: Schneider Electric Egypt and North East Africa