{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the ATV600 and ATV900 Process Drive run multiple motors ?

Article available in these languages: Spanish

Issuse:
Running multiple motors with an ATV600 and ATV900.

Product Line:
ATV600 ATV900 Altivar Process Drive

Environment:
All

Cause:
To simplify application

Resolution:
Yes, you can run multiple motors on a single drive.  Each motor will need separate external overload protections.
Both motors will share the same operations,  the start/stop and speed reference controls.
The heavy duty version of the drive should be sized according to the sum of both the horsepower and full load amps of both motors.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Schneider Electric Egypt and North East Africa