{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
In Vijeo Designer, can I access the properties of the Numeric Display object to lock-out or allow the input mode from scripting?

Issue
In Vijeo Designer, can I access the properties of the Numeric Display object to lock-out or allow  the input mode from scripting?

Product Line
Vijeo Designer

Environment
HMI Programming Software

Resolution
No, there are no scripting methods that will allow you to lock-out or allow  the input mode of the numeric display object.  A work-around would be to use the Security feature and set a Security Level for the numeric display object, or set Visibility on an Rectangle with Invisible Colour drawn on top of the Numeric Display.

Schneider Electric Egypt and North East Africa