Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to connect the ATV312HU40N4 to XMLG010D21 sensor in order to operate the VSD directly through the sensor's output signal ?

Article available in these languages: Japanese

The pressure sensor XMLG is of 2 wire connection; The (+ve inp)  wire is going to be connected to an input voltage of +24VDC and the other wire (output) is gong to be connected to the ATV312 Drive to the (slot AI3), So The speed can be varied depending on the Analog current output of the sensor.

Then, to configurate the Drive to work under this situation, Press on (Mode) button > choose (Ctl) > Press (Fr1) > choose (AI3) and make a long Press...

So, Now under any pressure from 0...10 bar (pressure setting range), A signal is going to be sent to the Drive to control its speed depending on the value of Analog output current (4-20mA)

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: