{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Vamp 255 communications maps

Issue
Need the register list for my VAMP relay.

Product Line
Vamp 255

Resolution
See the attached files for the VAMP 255 communications maps, this includes maps for:
Modbus
Profibus
SPA bus
DNP3
IEC101
IEC103
Modbus Master
ProfibusDP

Note: Latest information is available in m.vamp.fi

Schneider Electric Egypt and North East Africa

Attachment(s)

vamp255_fw10_108_motor_IEC103.xlsxvamp255_fw10_108_motor_IEC103.xlsx [17.54 KB]
vamp255_fw10_108_motor_ProfibusDP.xlsxvamp255_fw10_108_motor_ProfibusDP.xlsx [20.89 KB]
Modbus parameters.pdfModbus parameters.pdf [492.2 KB]
Modbus Profibus SPA bus Events.pdfModbus Profibus SPA bus Events.pdf [889.01 KB]
SPA bus data mappings.pdfSPA bus data mappings.pdf [931.58 KB]
vamp255_fw10_108_feeder_DNP3.xlsxvamp255_fw10_108_feeder_DNP3.xlsx [17.41 KB]
vamp255_fw10_108_feeder_IEC101.xlsxvamp255_fw10_108_feeder_IEC101.xlsx [18.39 KB]
vamp255_fw10_108_feeder_IEC103.xlsxvamp255_fw10_108_feeder_IEC103.xlsx [18.1 KB]
vamp255_fw10_108_feeder_ModbusMaster.xlsxvamp255_fw10_108_feeder_ModbusMaster.xlsx [10.49 KB]
vamp255_fw10_108_feeder_ProfibusDP.xlsxvamp255_fw10_108_feeder_ProfibusDP.xlsx [21.27 KB]
vamp255_fw10_108_motor_DNP3.xlsxvamp255_fw10_108_motor_DNP3.xlsx [17.41 KB]
vamp255_fw10_108_motor_IEC101.xlsxvamp255_fw10_108_motor_IEC101.xlsx [18.4 KB]
vamp255_fw10_108_motor_ModbusMaster.xlsxvamp255_fw10_108_motor_ModbusMaster.xlsx [10.5 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.