Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Why there is a difference in the Service breaking capacity (Ics) values of manually and electrically operated Compact NS>630.
The difference is due to the design of the Circuit Breakers. The Compact NS>630 manual basic frame (bloc cut) is different from NS electrical basic frame (bloc cut).
Ics depends on breaker type. Electrically operated Compact NS>630 is developed from Masterpact NT breaker because there is no option for adapting the motor mechanism on Compact NS>630.
The breaking performances of NT are less than Compact NS, hence it cannot be declared that the Ics values of electrically operated Compact NS>630 is same as manually operated Compact NS>630.
This is the reason why the service breaking capacity (Ics) values of manually operated and electrically operated Compact NS>630 MCCB are different.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: