Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Can an impulse-type power supply be used for electrical opening and closing order of Compact NS MCCB ?
Yes, the impulse-type power supply (time duration > 20 ms and Voltage level above 0.7Un) can be used for electrical opening and closing of Compact NS MCCB.
The power supply during the closing order is also impulse-type as the closing order is in series with the "Ready to close" switch. Hence even if the power supply is cut-off the breaker will close.
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Product:
Explore more
Product: