{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the default directory for ICD files installed with the SFT common library?

Issue
Need the default ICD file for a SEPAM relay.

Product Line
CET850
ICE61850

Resolution
The default directory is as follows:

Install drive (Typically C) > Program Files (X86) (Only X86 if installed on a 64-bit operating system) > Schneider > SFTCommon > IEC61850 > Edition_1 > ICD

This directory contains all of the ICD files that CET850 contains.

Schneider Electric Egypt and North East Africa