Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the thickness of the Steel sheet metal of Blokset Panel.
The Steel sheet metal thickness used in Blokset Panel is as per the below table:
Blokset Steel sheet metal thickness
Housing | Thickness mm |
Door | 2.00mm |
Rear panels | 2.00mm |
Side panels | 2.00mm |
Roof/Top | 2.00mm |
Frame | 2.00mm |
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: