{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why might a shunt trip breaker trip in a Motor Control Center with an ATS22 soft start?

Article available in these languages: Spanish

Issue:
Shunt trip accessory to the main breaker is tripping


Product Line:
ATS22 Soft Start

Environment:
Motor Control Centers using an ATS22 Soft Start with a shunt trip breaker

Cause:
Time delay relay is set to the wrong time.

Resolution:
Increase the time on the time delay relay.  This relay is used to delay the energization of the shunt trip coil when the bucket is powered ON.  The shunt trip coil must not be allowed to energize until the normally closed trip relay on the soft start has time to open.  Also, if the ATS22 goes to a faulted state, the shunt trip will trip the breaker.

Schneider Electric Egypt and North East Africa