Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the minimum opening time & closing time for the LF Circuit Breaker.
Schneider Make Circuit Breakers are designed on mean opening time or closing time.
The value is same for LF1 or LF2 or LF3 Circuit Breakers. It is linked to the operating mechanism RI used for all the LF Circuit Breaker.
- Mean opening time at Un : 48 ms.
- Mean Closing time at Un: 65 ms.
Where Un = Nominal Voltage
The minimum opening time and closing time values cannot be defined as these depend on the adjustment made during the short-circuit breaking tests.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: