{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the value of one minute power frequency withstand voltage for NSX Breaker?

Compact NSX range has Uimp of 8 kV. Following IEC-60947-1 / 60947-2 standard, 1,2/50 us impulse wave and power-frequency withstand voltage test are performed on the breaker.

For the power-frequency withstand voltage test at 50 Hz, the voltage depends on the rated insulation voltage Ui (as illustrated in attached document), which is 800V for Compact NSX:
Rated insulation voltage Ui : AC test voltage (R.M.S)
60 < Ui ≤ 300 : 1500
300 < Ui ≤ 690 : 1890
690 < Ui ≤ 800 : 2000
800 < Ui ≤ 1000 : 2200
So for Compact NSX the value of this voltage is 2000 V for 1 minute.

Schneider Electric Egypt and North East Africa

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.