Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
With view only client of Vijeo Citect 7.40, is there any limitation of windows/internet explorer related to the view only client ?
Version 7.40 has been tested to run on:
· Windows® 8 (32 and 64 bit)
· Windows® Server 2012
· Windows® 7 SP1 (32 and 64 bit)
· Windows® Server 2008 R2 SP1
· Windows® Server 2008 SP2 (32 and 64 bit)
Notes:
· Internet Explorer Version 7 or later is the minimum requirement when using the Process Analyst, Citect Web Client, or Citect Web Server. However, in line with Microsoft advice, we recommend you use the latest version of Internet Explorer, for correct functionality of these products.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: