Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the definition of the Voltage/Current labels on relay RXM4AB2GD ?

Definitions for each (Voltage/ Current) Label on the Relay

 
1. 125 VDC - It is "Control circuit voltage" or "Coil voltage of relay" 
 
2. 6A/ 250 VAC - It is mentioning the capacity of relay contact. The 6 Amps maximum current allowed at 250VAC as per IEC standard. 
 
3. Ul Ratings: 6A/ 277 VAC, 8A/ 30 VDC - It is mentioning the rating of relay contacts as per UL standard. 
 
4. 1/3 HP/ 120 VAC - It is B300 Pilot duty rating at 120VAC. The B300 rating is termed "pilot duty" which means it is for a specific highly inductive load 
 
5. 1/2 HP/ 250 VAC - It is B300 Pilot duty rating at 250VAC. The B300 rating is termed "pilot duty" which means it is for a specific highly inductive load. 
 

Schneider Electric Egypt and North East Africa

Attachment(s)
IMG-20140311-WA0002.jpg [62.07 KB]
IMG-20140311-WA0003.jpg [57.87 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: